AXIS#.MOTOR.IMID

Description

This parameter is the preset rotor flux building current for closed loop induction motor control (AXIS#.MOTOR.TYPE = 4).

The value of AXIS#.IL.IMID can be estimated using the motor name plate information.

The following rule should generally be used:

Id root-mean-square approximately equals lr multiplied by the square root of 1 minus open parentheses cos phi close parentheses squared multiplied by 0.8

In which Id is the value for AXIS#.IL.IMID, the preset rotor flux building current, Ir is the name plate phase current, cosϕ is the name plate power factor at rated and operation, and 0.8 is an empirical factor (accounts for the angle error due to voltage drop on the leakage induction).


  • This parameter is required to be configured for AXIS#.MOTOR.TYPE = 4

Context

For more information see Motor.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Arms

Range

0 to DRIVE.IPEAK

Default Value

0

Data Type

Float
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
AXIS1.MOTOR.IMID

500bh

0ah

Unsigned16

-

1000:1

Read/Write

No

AXIS2.MOTOR.IMID

510bh

0ah

Unsigned16

-

1000:1

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.MOTOR.IMID

6229

1855

Unsigned16

Read/Write

-

AXIS2.MOTOR.IMID

71765

1185

Unsigned16

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.MOTOR.IMID

6229

Float

Read/Write

-